[Medini files]S32K3xx customized FMEDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[Medini files]S32K3xx customized FMEDA

跳至解决方案
2,658 次查看
BoxLi
NXP Employee
NXP Employee

Hi:

Just want to confirm that whether we could release K3xx fmeda Medini file to customer?

  • If yes, does MediniAnalyze version must be 2021 R2?
  • If yes, could be via secure file or other ways?

My customer baught Ansys Mediti tool already, they want to make FMEDA with their own configuration.

Thanks a lot.

 

标签 (1)
标记 (1)
0 项奖励
1 解答
2,630 次查看
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

在原帖中查看解决方案

0 项奖励
2 回复数
2,631 次查看
Yashwant_Singh
NXP Employee
NXP Employee

Hello,

Yes the medini files for the S32K3xx family are available upon requests. Ansys release different version each year so the .mprx files for different products in the family are available under different versions however Medini allows migrating files to newer versions of the tool and so we would recommend using the latest one (2023 r2 or newer).

Secure files is the official channel for release however it can also be done via a common sharepoint link or drive with the customer.

Thanks!

-Yashwant

 

 

0 项奖励
2,610 次查看
BoxLi
NXP Employee
NXP Employee

Hi Yashwant:

Got it, thanks a lot.

0 项奖励