In FMEDA, for the following example with PTA0, what are the difference between two capture?
The capture1 is more like inside of the circuit for PTA0 in the MCU.
Also the capture2 is the external interface , which is limited to Pin.
My understanding is correct?
Capture1
Also for Capture1, there are the failure modes. Can you also explain it more detail? I could guess however I need more explicit explain for each meaning of the failure mode. For example, floating, stuck , pull up, pull down are understandable however, Inadequate Drive Strength/Slew Rate and incorrect dynamic range are not understandable that needs more additional information/explain. Also even understandable failure modes, we need further explain when those failure modes shall be used like input or only output and so on.
And the above Capture1 is MCU dependent on which is not supposed to be covered by the mechanisms such as the following? I think application shall consider the failure modes and use proper safety mechanisms?
• SM4.COMM_SAFEPROT
• SM1.RED_PERI_PHY_SEP
The below is pin that is more relevant to application.
Capture 2
The product is 32K388.
Hello Heeboem,
Please see some responses below:
Hoping this helps.
Thanks!
-Yashwant
Hello Mr. Park,
Can you please tell us which product you are referring to? THat will help me answer your question.