9S12VR & MC9S12G - ISO26262?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12VR & MC9S12G - ISO26262?

312件の閲覧回数
marcuslim
NXP Employee
NXP Employee

Hi,

In MC9S12ZVMB and  MC9S12ZVML Reference Manual, they stated that “  is targeted for safety Relevant System and is ISO26262 compliant development under NXP Safe Assure Program”

 

Searching in 9S12VR and MC9S12G Reference Manual, they  do not state about ISO26262 compliance

 

Thus will like to seek confirmation if 9S12VR and MC9s12G are  compliant to ISO26262?

Regards,

Marcus

ラベル(1)
0 件の賞賛
3 返答(返信)

290件の閲覧回数
aarul
NXP Employee
NXP Employee

Hi Marcus

Please have a look at following link:

https://community.nxp.com/docs/DOC-335435 

to see if you can find the information you are looking.

Regards

-Aarul

0 件の賞賛

290件の閲覧回数
marcuslim
NXP Employee
NXP Employee

Thanks Aarul !

Am I right to say that if the part is not listed in the indicated page, it means that the part is not compliance to ISO26262?

Regards,

Marcus

0 件の賞賛

290件の閲覧回数
aarul
NXP Employee
NXP Employee

I suggest that you should check the product documentation to find whether a product is ISO26262 compliant or not instead of relying on the list on the Safeassure Community. If in doubt feel free to ask in the forum.

0 件の賞賛