9S12VR & MC9S12G - ISO26262?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12VR & MC9S12G - ISO26262?

923 Views
marcuslim
NXP Employee
NXP Employee

Hi,

In MC9S12ZVMB and  MC9S12ZVML Reference Manual, they stated that “  is targeted for safety Relevant System and is ISO26262 compliant development under NXP Safe Assure Program”

 

Searching in 9S12VR and MC9S12G Reference Manual, they  do not state about ISO26262 compliance

 

Thus will like to seek confirmation if 9S12VR and MC9s12G are  compliant to ISO26262?

Regards,

Marcus

Labels (1)
0 Kudos
3 Replies

901 Views
aarul
NXP Employee
NXP Employee

Hi Marcus

Please have a look at following link:

https://community.nxp.com/docs/DOC-335435 

to see if you can find the information you are looking.

Regards

-Aarul

0 Kudos

901 Views
marcuslim
NXP Employee
NXP Employee

Thanks Aarul !

Am I right to say that if the part is not listed in the indicated page, it means that the part is not compliance to ISO26262?

Regards,

Marcus

0 Kudos

901 Views
aarul
NXP Employee
NXP Employee

I suggest that you should check the product documentation to find whether a product is ISO26262 compliant or not instead of relying on the list on the Safeassure Community. If in doubt feel free to ask in the forum.

0 Kudos