SPC5607 base failure rate and failure split for FMEDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5607 base failure rate and failure split for FMEDA

639 Views
harald_truebswe
Contributor I

Hello,

I have some questions regarding SPC5607 / SPC5605 and FMEDA according to ISO26262.

We are developing an ECU with an ASIL B safety goal and therefore we are building a FMEDA for the ECU.

Can you provide me the base failure rate of this SPC which we should use in our analysis and also the reference temperature for this failure rate?

Our FMEDA is actually built with data of Siemens SN29500 and the failure split according to Birolini.

Do you have also some hints to model the failure split?

According to Birolini we actually calculate with 60% open, 10% short to GND, 10% short to VCC (pin failures) and 20% functional failures (core, memory, ADC, core supply, clock).

From Mr. jochengerster we also got the FMEDA from the µC itself.

Best regards

Harald Trüswetter

0 Kudos
1 Reply

562 Views
aarul
NXP Employee
NXP Employee

Dear Harald

Based on our discussion and response from NXP, I hope your queries were answered.

Regards

-Aarul

0 Kudos