NXP SAF SquareCheck vs BIST Manager

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP SAF SquareCheck vs BIST Manager

Jump to solution
2,029 Views
EmmanuelDoit
Contributor II

Dear NXP safety experts, what is the difference between NXP SAF Square Check vs NXP SAF BIST manager? Both seem to perform tests, to detect latent failures in safety mechanism which detect random HW failures.

Tags (1)
0 Kudos
1 Solution
2,014 Views
naveenm
NXP Employee
NXP Employee

Hi,

Please find the answers below:

Q1. Can you specify which S32G2 HW modules are covered by the NXP SAF SquareCheck vs BIST Manager?

A1. A detailed list of H/W modules covered under SCheck can be found in Table 4. S32G Test Targets Description under section 2.2.1 in S32G2 SAF SquareCheck User Manual Rev. 7 — 25 June 2021. 

A detailed list of H/W modules covered under Chapter 72 Self-Test Control Unit (STCU2) section 72.1.3 and 72.1.4 of S32G2 Reference Manual, Rev. 4, October, 2021

Q2. Can you confirm if both the NXP SAF SquareCheck & BIST Manager are necessary (or recommended) for using S32G2 in ASILB application?

A.2) It is recommended to run SquareCheck and BIST for ASIL B application. Run SquareCheck on safety mechanism and BIST on rest of the logic. The BIST can additionally be run on safety mechanism if there is low DC achieved through corresponding SquareCheck element.

 

Hope it helps.

Regards,

NaveenM

View solution in original post

0 Kudos
3 Replies
2,024 Views
naveenm
NXP Employee
NXP Employee

Hi Emmanuel,

SquareCheck tests the H/W safety mechanisms whereas BIST (LBIST and MBIST) tests the entire logic of the chip which may include the H/W safety mechanism as well.

Hope it helps.

Regards,

NaveenM

0 Kudos
2,022 Views
EmmanuelDoit
Contributor II

Dear NXP, thanks for you answer. Could you provide a little more information?

Q1. Can you specify which S32G2 HW modules are covered by the NXP SAF SquareCheck vs BIST Manager?

Q2. Can you confirm if both the NXP SAF SquareCheck & BIST Manager are necessary (or recommended) for using S32G2 in ASILB application?

0 Kudos
2,015 Views
naveenm
NXP Employee
NXP Employee

Hi,

Please find the answers below:

Q1. Can you specify which S32G2 HW modules are covered by the NXP SAF SquareCheck vs BIST Manager?

A1. A detailed list of H/W modules covered under SCheck can be found in Table 4. S32G Test Targets Description under section 2.2.1 in S32G2 SAF SquareCheck User Manual Rev. 7 — 25 June 2021. 

A detailed list of H/W modules covered under Chapter 72 Self-Test Control Unit (STCU2) section 72.1.3 and 72.1.4 of S32G2 Reference Manual, Rev. 4, October, 2021

Q2. Can you confirm if both the NXP SAF SquareCheck & BIST Manager are necessary (or recommended) for using S32G2 in ASILB application?

A.2) It is recommended to run SquareCheck and BIST for ASIL B application. Run SquareCheck on safety mechanism and BIST on rest of the logic. The BIST can additionally be run on safety mechanism if there is low DC achieved through corresponding SquareCheck element.

 

Hope it helps.

Regards,

NaveenM

0 Kudos