EIM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM

1,125件の閲覧回数
HeebeomPark
Contributor II

In the FMEDA, there is no safety mechanism for EIM1/2/3 and the comment is written like "EIM cannot be activated with a single bit.". In this case, what is the recommendation for safety application?

Can you explain in more detail? 

HeebeomPark_0-1717631835087.png

 

0 件の賞賛
1 返信

998件の閲覧回数
antoinedubois
NXP Employee
NXP Employee

Hello,

EIM are the feature to test the safety mechanisms therefore if they fail they would be consider triple point fualt and are consider safe.

The only potential failure mode is the unintended activation of the EIM, however in the HW there is a dual enable and Triple voting flogs therefore it cannot happen. There is no specific implementation required by the customer it is built into the HW.

0 件の賞賛