Difference between ASILs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between ASILs

931 Views
oscar_hinojosa
Senior Contributor II

Hello Safety team,

Will we have somewhere a table of what each of the ASIL should have?

For example in the Safety Manual of S32k1XX mention for safety, you need to use a redundant watchdog system, and for that, you need to use an External Watchdog and have a monitor but this is applicable for ASIL B or also ASIL A.

Thanks

Oscar Hinojosa.

Note:- If this post answers your question, please click the Accept as Solution button.
Thank you!
Best regards,
Oscar Hinojosa.
-
Labels (1)
0 Kudos
1 Reply

881 Views
aarul
NXP Employee
NXP Employee

Hi Oscar

I don't think we can have such a table as the ASIL x is dependent on application usecase in Safety Manual. We do provide dynamic FMEDA with some capability of changing the target ASIL and meet the random fault metric by selecting appropriate safety mechanism.

However, the selection of the right safety mechanisms is safety analysis of the application and implementation at system level.

The WDOG is an important mechanism to avoid dependent failures and the Safety Manual advises on the kind of failures it is covering as well as guidelines on different ways to implement it (for example, any monitor that can cover for loss of communication with microcontroller).

Hope this helps,

Regards

-Aarul

0 Kudos