Custom DFMEA Errors - MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom DFMEA Errors - MPC5777C

ソリューションへジャンプ
1,525件の閲覧回数
davidfantl
NXP Employee
NXP Employee

 Hello,

I am working on a custom DFMEA for the MPC5777C. I am trying to create a customer version of the summary (FMEDA_MPC5777C_Summary_INTERNAL_rev_1_0.xlsm). I am getting the following errors. 

 

davidfantl_0-1668425053636.png

 

0 件の賞賛
1 解決策
1,516件の閲覧回数
davidfantl
NXP Employee
NXP Employee

Thanks for the excellent support Bhavik.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,517件の閲覧回数
davidfantl
NXP Employee
NXP Employee

Thanks for the excellent support Bhavik.

0 件の賞賛
1,521件の閲覧回数
nxf65498
NXP Employee
NXP Employee

Hi Dave,

You are getting this error because the full path in FMEDA files aren't matching with path where these file are locally available in laptop. I would request you to please check the location of file path exactly matches with FMEDA files. If error still persist then may be we can have call or you can share the FMEDA files.

I hope this helps.

Best regards,

Bhavik Vakhariya  

0 件の賞賛