How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip"

1,068 Views
Lvyang508
Contributor I

Hi ,

   I installered "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite" from GreenVIP, but I could not find it in the following screenshot.

Lvyang508_0-1768890302700.png

If I installered it again, there was a error tip.

Lvyang508_1-1768890483163.png

Please help me.

 

Thank you!

 

0 Kudos
Reply
6 Replies

1,052 Views
Joey_z
NXP Employee
NXP Employee

Hi,Lvyang508

Please check your RTD version, it seems a conflict between the RTD and RTOS package.

Also, what is the version of S32DS IDE are you using?

BR

Joey

0 Kudos
Reply

1,045 Views
Lvyang508
Contributor I
  1. S32DS IDE: S32DS for Platform 3.6.5
  2. I downloaded the corresponding package and installered according to UG_S32ZE_GreenVIP.pdf

Lvyang508_0-1768894395722.png

 

0 Kudos
Reply

1,041 Views
Joey_z
NXP Employee
NXP Employee

Hi,Lvyang508

Thank you for your reply.

Do you have installed the SW32ZE_RTD_R21-11_2.0.1_D2505_
DesignStudio_updatesite.zip in the S32DS IDE?

Joey_z_0-1768901138801.png

BR

Joey

0 Kudos
Reply

923 Views
Lvyang508
Contributor I

Hi Joey,

     I have installed the SW32ZE_RTD_R21-11_2.0.1_D2505_
DesignStudio_updatesite.zip in the S32DS IDE.

Lvyang508_0-1769124772985.png

Thanks!

 

0 Kudos
Reply

915 Views
Joey_z
NXP Employee
NXP Employee

hi,Lvyang508

Thank you for your reply.

This issue may be caused by the version conflict. Please try to use the S32DS IDE 3.6.1 to refer to the UG_S32ZE_GreenVIP.pdf.

Joey_z_0-1769135356228.png

BR

Joey

828 Views
Lvyang508
Contributor I

Hi Joey,

     Thanks for your reply.

      I have installed S32IDE 3.6.1, but the problem still remain.

Lvyang508_0-1769311052784.png

Lvyang508_1-1769311085792.png

 

BR,

 

0 Kudos
Reply