Hi ,
I installered "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite" from GreenVIP, but I could not find it in the following screenshot.
If I installered it again, there was a error tip.
Please help me.
Thank you!
Hi,Lvyang508
Please check your RTD version, it seems a conflict between the RTD and RTOS package.
Also, what is the version of S32DS IDE are you using?
BR
Joey
Thank you for your reply.
Do you have installed the SW32ZE_RTD_R21-11_2.0.1_D2505_DesignStudio_updatesite.zip in the S32DS IDE?
Hi Joey,
I have installed the SW32ZE_RTD_R21-11_2.0.1_D2505_DesignStudio_updatesite.zip in the S32DS IDE.
Thanks!
hi,Lvyang508
This issue may be caused by the version conflict. Please try to use the S32DS IDE 3.6.1 to refer to the UG_S32ZE_GreenVIP.pdf.
Thanks for your reply.
I have installed S32IDE 3.6.1, but the problem still remain.
BR,