S32V234 Processor Temperature Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V234 Processor Temperature Sensor

3,735件の閲覧回数
sriramanravi
Contributor I

Hi,

We are using S32V234 Processor from NXP and are trying to read the temperature Sensor Values. It will be helpful if any one can provide any input on how to read Temperature Sensor Values for S32V234 on chip Temperature Sensor in U-Boot or Linux, is there already a driver for that?

Best Regards

Sriraman Ravi

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,375件の閲覧回数
tommalnar
Contributor III

For Linux there is a driver available at \drivers\thermal\s32v234_thermal.c as part of the kernel used in BSPv14.

0 件の賞賛
返信

3,375件の閲覧回数
rajeevr
Contributor I

Hi All,

Anyone knows the answer for the above question. Please reply it would be helpful.

0 件の賞賛
返信