Hi all,
I can't launch Ethernet service in S32V234EVB,it is shown below:
Stopping network...Starting network...
[ 230.805376] fec 40032000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=40032000.etherne:07, irq=-1)
[ 230.816964] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready.
I tried both Static IP and DHCP IP .
thanks
This should not be a problem.
What is the version of Linux BSP are you using?
Thanks.
HI,I have solved this problem,it perhaps something wrong in hardware ,we fixed the RJ45 interface,and it goes on well.Thanks for your answer!