I met problem in S32V Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I met problem in S32V Ethernet

1,591 Views
hnxiaojuzi
Contributor II

Hi all,

I can't launch Ethernet service in S32V234EVB,it is shown below:

Stopping network...Starting network...
[ 230.805376] fec 40032000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=40032000.etherne:07, irq=-1)
[ 230.816964] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready.

I tried both Static IP and DHCP IP .

thanks

Tags (1)
2 Replies

1,354 Views
KushalShahNXP
NXP Employee
NXP Employee

This should not be a problem.

What is the version of Linux BSP are you using?

Thanks.

0 Kudos
Reply

1,354 Views
hnxiaojuzi
Contributor II

HI,I have solved this problem,it perhaps something wrong in hardware ,we fixed the RJ45 interface,and it goes on well.Thanks for your answer!