Boot fail on S32V234 EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot fail on S32V234 EVB

3,729件の閲覧回数
erezsteinberg
Contributor IV

Hello experts,

(Sorry for putting in this space; the S32V space is disabled for some reason!)

I am having issues booting Linux on an S32V234-EVM (28899 Rev D).

I am using the pre-built images (I tried v16 and V17).

The problem seems to be with reading the partition table from the SDCARD. 

U-Boot 2016.01+ge19ad21 (Mar 03 2018 - 04:20:46 +0700)
aarch64-fsl-linux-gcc (Linaro GCC 6.3-2017.06~dev) 6.3.1 20170509
GNU ld (GNU Binutils) 2.27.0.20160806
switch to partitions #0, OK
mmc0 is current device
** No partition table - mmc 0 **
Booting from net ...

Even if I use TFTP to load the kernel and dtb to memory, and then try to boot with root=/dev/mmcblk0p2, then the Kernel fails with:

[ 11.200481] mmc0: Timeout waiting for hardware interrupt.
[ 11.206637] mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
[ 11.288416] mmc0: tried to reset card
[ 21.320499] mmc0: Timeout waiting for hardware interrupt.
[ 21.325631] mmcblk0: error -110 transferring data, sector 0, nr 8, cmd response 0x900, card status 0x0
[ 21.334861] mmcblk0: retrying using single block read

I tried 3 different brands SDCARDS, but I get the same result.

Any suggestions?

Thx,

Erez

タグ(1)
0 件の賞賛
返信
1 返信

3,371件の閲覧回数
KushalShahNXP
NXP Employee
NXP Employee

Hi Erez,

We have stopped supporting this community group. But we still support S32V2 question using our ticketing system.

Please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

 

Thank you for understanding.

 

Regards,

Kushal

0 件の賞賛
返信