EB Tresos - Ae module generating code with wrong SPI module selected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB Tresos - Ae module generating code with wrong SPI module selected

1,285 Views
guillermoarb
Contributor I

Ae plugin/module from RTD 6.0.0 is generating code to use SPI LSPI0 instead of LSPI1 this is not configurable and its wrong because Ae only can use SPI 1

Version

guillermoarb_4-1765482819745.png

 

 

 

SPI selection in Ae is not configurable

guillermoarb_0-1765482601509.png


Due to D2D connection SPI 1 need to be used 

guillermoarb_1-1765482669251.png


Nevertheless, generated file use SPI 0 

guillermoarb_2-1765482697557.png



This was modified manually as temporary solution

guillermoarb_3-1765482780229.png

 

Tags (3)
0 Kudos
Reply
1 Reply

1,267 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @guillermoarb 

Please verify the following:

  1. Open the AeSpiSequence tab in your configuration tool.
  2. Check that the AeSpiSequenceName is assigned to the correct SpiSequence.
  3. Confirm that this SpiSequence has its SpiJobAssignment linked to the appropriate SpiJob.
  4. Verify that the SpiJob has its SpiDeviceAssignment set to the SpiExternalDevice intended for the LPSPI1 instance.

If these instructions seem unclear or confusing, please refer to the example project Ae_Spi_Example_EB_001_S32M276, provided with the RTD, as it can help validate that there is no incorrect or missing configuration.

 

BR, VaneB

0 Kudos
Reply