why RTI interrupt can't triggle.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why RTI interrupt can't triggle.

Jump to solution
2,967 Views
KerryJ
Contributor II

I used the S32DS 3.4, Why PIT0_CH0 and PIT0_CH1 can generate a interrupt with the same configuration , but the PIT0_CH_RTI not?

0 Kudos
Reply
1 Solution
2,914 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi KerryJ,

This is an example, that you are needing.

Best regards,

Dan

View solution in original post

0 Kudos
Reply
4 Replies
2,950 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which device and which SDK/RTD is used?

Regards

Lukas

0 Kudos
Reply
2,941 Views
KerryJ
Contributor II

DEVICE IS

S32K344

AND RTD IS 

S32K3 RTD AUTOSAR 4.4 VERSION 2.0.0

0 Kudos
Reply
2,915 Views
DanNguyenDuy
NXP Employee
NXP Employee

Hi KerryJ,

This is an example, that you are needing.

Best regards,

Dan

0 Kudos
Reply
2,896 Views
KerryJ
Contributor II

Thanks you so much.

I find when I config PIT0_CH0 first, the PIT0_RTI is disabled, even though config RTI later, the RTI is still disabled.

You should config RTI first then config PIT0_CH0, which both RTI and CH_0 are useful.

Tags (1)
0 Kudos
Reply