use EBTRESOS 29 generate code and debug via S32DS for S32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use EBTRESOS 29 generate code and debug via S32DS for S32

2,589件の閲覧回数
BigSun
Contributor II

now try to use tresos 29 generate code, and debug via S32Design studio for s32. by example project in RTD3.0.0 

Softwares:

S32 design studio for s32, RTD3.0, TRESOS29.0

sample project used: S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Adc_TS_T40D34M30I0R0\examples\EBT\S32K3XX\Adc_example_S32K344

The code generation and compile passed. but when I debug the elf generated in S32DS IDE via a new debug configuration, following error occur. How configure IDE to solve this?

BigSun_0-1709531076193.pngBigSun_0-1709531076193.png

the debug configuration is:

BigSun_1-1709531135926.pngBigSun_1-1709531135926.pngBigSun_2-1709531167582.pngBigSun_2-1709531167582.png

BigSun_3-1709531299307.pngBigSun_3-1709531299307.png

 

 

 

 

 

 

 

 

0 件の賞賛
返信
1 返信

2,573件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the images you have shared, it seems that you are debugging with a JLink device with the default S32DS JLink debug configuration. As far as we understand, S32K3 RTD does not provide any debug support for JLink devices, just for PE Micro and the available debug interface under the S32K3 evaluation boards.

We can recommend contacting SEGGER support, since they should be able to better support this inquiry, since with the available debuggers we are able to debug the application from our side with no problem.

We do apologize.

Please, let us know.

0 件の賞賛
返信