urgent help needed: the project uplevel folder is gone while renaming the project in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

urgent help needed: the project uplevel folder is gone while renaming the project in S32DS

985件の閲覧回数
cranes
Contributor IV

Hello,

Using S32DS version 3.5, when I rename a project, the project is gone in S32DS, also not available in the hard disk any more. Not only that, the whole uplevel folder is gone with all the projects in that folder.

The operation is right clicking the project, then clicking "rename", a window pops up with the uplevel folder name. With a little hesitation, I still changed the name, then the whole uplevel folder is gone. Can this folder be found back, or it is completely deleted from the hard disk? 

What is the right operation to change a project's name?

Thanks!

Crane

0 件の賞賛
返信
2 返答(返信)

945件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have tried it on my end and it is working properly.

The folder should be officially there so it will propagate to .xml file

Best regards,

Peter

0 件の賞賛
返信

965件の閲覧回数
cranes
Contributor IV

It looks that it works fine to rename the project if the project is in the workspace folder. 

It happens when the project is in a subfolder in the workspace folder.

0 件の賞賛
返信