update S32DS plugin GNU ARM PEmicro interface OFFLINE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

update S32DS plugin GNU ARM PEmicro interface OFFLINE.

980 Views
zxdd
Contributor II

Hi~

When using S32DS, I found that the chip list of PEdebugger in the project configuration did not have the chip model I expected (s32k324_SECUREDEBUG). I want to upgrade the relevant plug-in version (GNU ARM PEmicro interface Debugging Support). Because I am in a limited network environment, I can only update offline. Where can I download the offline upgrade package of this plug-in?


thank you~

Tags (2)
0 Kudos
Reply
1 Reply

962 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I don't know which version of RTD you have installed, so I'm not sure which version of S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices I would recommend you install.

If you installed S32K3 RTD 3.0.0, please refer to the step3 of HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.
If you installed S32K3 RTD 4.0.0, please refer to the step3 of RTD 4.0 with Design Studio 3.5


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply