the question about the registers of flash controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the question about the registers of flash controller

1,511件の閲覧回数
langweihua1643
Contributor I

Hello 

Related to Flash memory , I found a conflict(maybe) need to support

In S32K14x Seriex Cookbook.pdf ,I found description as below:

It means ---> Value 1 means Enable , Value 0 means Disable;

But in S32K144_RM.pdf ,I found that 

the conflict is :Value 0 means enable, Value 1 means disable

So I am confused about this ,which is correct ? or if my undersood is wrong?

Thank you.

best regards

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,392件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The current reference manual rev.9 is correct.

Value 0 means enable, Value 1 means disable.

And the default out-of-reset configuration of OCM1 is 0b00 that means enabled.

It was the other way round on the first S32K144 maskset 0N77P.

Thank you for pointing this out.

Regards,

Daniel

0 件の賞賛
返信

1,392件の閲覧回数
langweihua1643
Contributor I

Hey,

Thank you for your reply very much!

0 件の賞賛
返信

1,392件の閲覧回数
langweihua1643
Contributor I

(the attached picture may be upload failed)the register of my question is MSCM->OCMDR0 and MSCM->OCMDR1

0 件の賞賛
返信