the code of Icu in Emios_Icu_Ip.c wastes lots of memeory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the code of Icu in Emios_Icu_Ip.c wastes lots of memeory

425件の閲覧回数
LewisThin
Contributor III

S32K3 RTD is 2.0.0 in Emios_Icu_Ip.c the variable eMios_Icu_Ip_ChState 's size is 5472 bytes, whose size is all of the icu channle resource and the field of the structure contains lots member which can be defined as const

タグ(1)
0 件の賞賛
返信
1 返信

387件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LewisThin,

RTD_ICU_RamSizeReport.xlsx

RTD_ICU_SizeReport.xlsx

can be found in SW32K3_RTD_4.4_2.0.0_D2203_QualityPackage.zip

Plese make sure the compiler options are set as per the SW32K3_RTD_4.4_2.0.0_D2203_ReleaseNotes.pdf

 

Regards,

Daniel

0 件の賞賛
返信