the code of Icu in Emios_Icu_Ip.c wastes lots of memeory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the code of Icu in Emios_Icu_Ip.c wastes lots of memeory

429 Views
LewisThin
Contributor III

S32K3 RTD is 2.0.0 in Emios_Icu_Ip.c the variable eMios_Icu_Ip_ChState 's size is 5472 bytes, whose size is all of the icu channle resource and the field of the structure contains lots member which can be defined as const

Tags (1)
0 Kudos
Reply
1 Reply

391 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LewisThin,

RTD_ICU_RamSizeReport.xlsx

RTD_ICU_SizeReport.xlsx

can be found in SW32K3_RTD_4.4_2.0.0_D2203_QualityPackage.zip

Plese make sure the compiler options are set as per the SW32K3_RTD_4.4_2.0.0_D2203_ReleaseNotes.pdf

 

Regards,

Daniel

0 Kudos
Reply