Thank you for your attention .
the demo use FULL_MEM firmware .
I tried it again like you said , use the default script (c:\T32\demo\arm\flash\s32k3.cmm) already sets area 0x7D_4000 - 0x7F_FFFF as NOP in s32k344 development board ( installed the Hse firmware). the software project is a non-HSE software project as mentioned earlier.
when download the app, it has a "checking flash" message, then trigger a error "FLASH programming error around address c:0x10000000" in lauterbach emulator / trace 32.
then i add the statements to this script like below.
FLASH.ChangeType 0x1B000000--0x1B001FFF NOP
FLASH.ChangeType 0x10000000--0x10000100 NOP
FLASH.ChangeType 0x10017FFF--0x1001FFFF NOP
the app can be downloaded into the mcu successfully . meanwhile ,it can be running online in trace32.
but when i RESetOut in the trace32, it can't finished the job normally(reset the mcu). when i "run/go" in trace32, it will trigger a "Hardfault_handler". somtimes , it stop in "sys_m7_cache_init()" . power off and resart the s32k344 development board, then "attach" in trace32, it can be running again.

but i debug the same non-HSE software project as mentioned earlier use a PE/USB MULTILINK, it can be downloaded normally, and it can be debug normally include "reset / run" in s32ds.
As described above, is there a problem with the script of lauterbach/trace32 ?