I am working on s32k324 controller. I wanted to use the uart using the DMA.I am trying to send 10 bytes of data, but I am able to send only one byte of data.
when i am using the function
"Lpuart_Uart_Ip_GetTransmitStatus(3,&remainingBytes)"
the return value is "LPUART_UART_IP_STATUS_BUSY" and remainingBytes bytes is reduced by one (9).
i am able to transmit one byte of data only when i change the Second parameter in the below function
Dma_Ip_SetLogicChannelCommand(UartUserCfg->TxDMAChannel, DMA_IP_CH_SET_HARDWARE_REQUEST);
the above function is auto generated.
In the below function second parameter is changed for which i am able to transmit one byte.
Dma_Ip_SetLogicChannelCommand(UartUserCfg->TxDMAChannel, DMA_IP_CH_SET_SOFTWARE_REQUEST);
I have also attached the code below. I want some support, plz help me out,
thanks in advance
解決済! 解決策の投稿を見る。
hi Petr,
It's working
Thanks for the support
hi petr
It is working. thank you
Hi Petr,
Thanks for the support. I am able to transmit and receive the data using DMA
Thanks PetrS,
I had take the your project as the reference.
But i am not able to transmit any data.
i am trying to send the data using "lpuartStatus = Lpuart_Uart_Ip_AsyncSend(3, (uint8_t*)arrys, 5);"
The return value is always "LPUART_UART_IP_STATUS_SUCCESS".
I am getting event as "LPUART_UART_IP_EVENT_TX_EMPTY" for event call back function mentioned below.
UART_event_cbk(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData);
can you Please guide me
Hi,
seems below thread gives very basic LPUART DMA example using RTD:
https://community.nxp.com/t5/S32K/S32K3-LPUART-using-DMA-in-RTD-3-0-0/m-p/1737356
BR, Petr