s32k312

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k312

2,067 Views
fengba_360
Contributor III

I'm using SDS3.5 to program the S32K312. When I burn the program through debugging, the CPU fails to run and reports an error as shown in the image, which seems like it's not entering the main function. Could you help me diagnose the possible reasons? The attached file is the project engineering.  

sds32version :3.5    sdk version:* Build Version : S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331

微信图片_20240828181611.png微信图片_20240828181605.png

0 Kudos
Reply
3 Replies

1,908 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @fengba_360,

Do you have an NXP EVB or your own custom board?

Does it happens with all SDK/RTD examples that have not been modified in any way?

 

Thanks,

Daniel

0 Kudos
Reply

2,009 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @fengba_360,

I just loaded your .elf to the MCU, so I did not compile the project.

And I don't have the behavior you reported.

danielmartynek_0-1725017445272.png

 

Do you see this when you load an NXP example too?

Can you share the debug configuration?

 

Thanks,

BR, Daniel

 

 

0 Kudos
Reply

2,002 Views
fengba_360
Contributor III

I still have this problem when loading the NXP s32k312 example routine. I have tried to replace the J-Link debugging tool, but the situation remains the same.

 

微信图片_20240831130155.png微信图片_20240831130126.png

0 Kudos
Reply