s32k312 configure error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k312 configure error

482 Views
xiaodinghuang
Contributor II

When I open the S32K312 project, it shows that it can't generate code. I feel like my SDK is fine, not sure what the reason is. But my friend is ok, he is used 3.6.4 version, i used 3.6.1

xiaodinghuang_2-1786612023313.png

 

 

 

Tags (1)
0 Kudos
Reply
4 Replies

440 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @xiaodinghuang 

Which RTD version are you currently using?

If you hover the mouse pointer over the error message, do you see any more detailed description of the error?

Was the project created from scratch in S32DS 3.6.1, imported from an RTD example, or migrated from a different S32DS version?

Have there been any recent changes to the project  or your S32DS installation before this issue started occurring?

 

BR, VaneB

0 Kudos
Reply

431 Views
xiaodinghuang
Contributor II
Spoiler
xiaodinghuang_0-1786671953881.png

this is error log,but i dont find good solution

0 Kudos
Reply

432 Views
xiaodinghuang
Contributor II

no, i never change s32ds configure, the project is migrated from others, RTD is SW32K3_RTD_4_4_2_0_2_D2211, is same with the project, i open my local project is ok

Tags (1)
0 Kudos
Reply

404 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @xiaodinghuang 

Thank you for sharing the information.

Please note that RTD version 2.0.2 is not officially compatible with S32DS 3.6.x releases. This RTD version was developed and validated specifically for S32DS 3.4, so using it with a newer S32DS version is not recommended.

We cannot guarantee correct functionality or behavior, as this combination was not tested or qualified. To avoid potential compatibility issues, we recommend using the RTD version with the S32DS release for which it was originally designed and validated.

0 Kudos
Reply