s32k312 Interrupt priority

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k312 Interrupt priority

1,296件の閲覧回数
fengba_360
Contributor III

Hello, I am currently enabling a peripheral interrupt using the following method. I would like to ask how to set the interrupt priority for this peripheral in this particular way.

Is there a corresponding interface function?

The SDK I am using is S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331.

can:
IntCtrl_Ip_EnableIrq(FlexCAN1_1_IRQn);
IntCtrl_Ip_InstallHandler(FlexCAN1_1_IRQn, CAN1_ORED_0_31_MB_IRQHandler, NULL_PTR);
pit:
IntCtrl_Ip_EnableIrq(FlexCAN1_2_IRQn);
IntCtrl_Ip_InstallHandler(FlexCAN1_2_IRQn, CAN1_ORED_32_63_MB_IRQHandler, NULL_PTR);
 
 
IntCtrl_Ip_InstallHandler(PIT0_IRQn, PIT_0_ISR, NULL_PTR);
IntCtrl_Ip_EnableIrq(PIT0_IRQn);
0 件の賞賛
返信
1 返信

1,273件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @fengba_360,

There are these APIs:

danielmartynek_0-1734598325326.png

 

Regards,

Daniel

0 件の賞賛
返信