s32k3 secure debug interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3 secure debug interface?

Jump to solution
2,774 Views
victory
Contributor V

Hi Nxp,

    i've set S32K312  LC to OEM_PROD and secure debug is active.  i only got jlink now and have some question :

1. to open the secure debug,  is interface JTAG / SWD both available or ONLY JTAG?

2. is there any scripts for jlink to authurize secure debug?  

0 Kudos
Reply
1 Solution
2,728 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @victory 

1. To open secure debugging, are JTAG/SWD or JTAG ONLY interfaces available? Both JTAG and SWD interfaces are available.

2. Is there any script for jlink to enable secure debugging? I am afraid J-Link does not support secure debugging of applications with password authentication or with challenge/response authentication.

 

BR, VaneB

View solution in original post

0 Kudos
Reply
2 Replies
2,729 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @victory 

1. To open secure debugging, are JTAG/SWD or JTAG ONLY interfaces available? Both JTAG and SWD interfaces are available.

2. Is there any script for jlink to enable secure debugging? I am afraid J-Link does not support secure debugging of applications with password authentication or with challenge/response authentication.

 

BR, VaneB

0 Kudos
Reply
2,703 Views
victory
Contributor V
thanks, use pylink to implement CR auth works.
0 Kudos
Reply