s32k3 hse advanced secure boot debug best practice?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3 hse advanced secure boot debug best practice?

1,290 Views
victory
Contributor V

during LC in cust_del, if i modified the flash and reset the mcu,  hse smr check maybe stop the app code run due to che check failed?  how to recover the mcu, for example ,clear the SMR/CR record when app code not run? is there any best practice workflow for debug secure boot ?

0 Kudos
Reply
2 Replies

1,266 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I don't understand this question.

During CUST_DEL, APP Debug port is open, No restriction for Application development, HSE Debug Port Closed

Could you describe your question a bit clearer? Thanks

0 Kudos
Reply

1,247 Views
victory
Contributor V
if i configured SMR/ CR and use S32DS+JTAG to program and debug code, each time after i've programed the code and reset, will the hse hold the core0 reset due to SMR check failed, and my code cant run? or in CUST_DEL stage and JTAG connected, the hse SMR will not check the flash the code can run normally?
0 Kudos
Reply