s32k3 OTA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32k3 OTA

1,710 次查看
youxi
Contributor IV

Hi:

After these steps are complete, what is the process of performing an OTA upgrade?

youxi_0-1702970020777.png

 

标记 (1)
0 项奖励
回复
1 回复

1,680 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Step 2 starts to OTA program the new application App_v2, and step 6 starts to run App_v2. This AN did not program a real new application, just used the copied application(App_v1) as a new application(App_v2) to demonstrate.

2. Detect that no valid program exists in the passive partition, copy the same data as the active
partition to the passive partition, which is Cfg_v1 and App_v1 program code.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复