s32k146evb CAN_PAL example issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s32k146evb CAN_PAL example issue

跳至解决方案
2,230 次查看
yfliu
Contributor IV

Got an offical s32k146 EVB board, created sample project from can_pal_s32k146 example, checked it from another commercial USBCAN box.

The USBCAN box complains sending error, which happened a lot with another board when the TJA1044 transceiver on that board was not enabled.

I am wondering if the UJA1169 transceiver on the official k146 EVB is not enabled by default? 

 

0 项奖励
回复
1 解答
2,224 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi yfliu,

About how to use the SDK example, please refer the answer in CAN communication on s32k148EVB-Q144
The setting may different between S32K146EVB and S32K148EVB, you need to check the example and documentation of S32K146EVB. 

Notice external 12V power adapter is needed.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,225 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi yfliu,

About how to use the SDK example, please refer the answer in CAN communication on s32k148EVB-Q144
The setting may different between S32K146EVB and S32K148EVB, you need to check the example and documentation of S32K146EVB. 

Notice external 12V power adapter is needed.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,221 次查看
yfliu
Contributor IV

Robin,

Used a 9V power adaptor for the K146EVB and now it works! Many thanks!

Previsouly I tried the example with another K144 customer board using just USB power, so wasn't aware of the importance of the power supply for CAN interface on K146EVB board.

yfliu

 

 

 

0 项奖励
回复