s32k144 low voltage detection interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k144 low voltage detection interrupt

1,923件の閲覧回数
SivaB
Contributor III

Any sample code is available for low voltage detection interrupt for S32K144.

How to configure LVD interrupt in CT.

Used RTD version: SW32K1_RTD_4_4_1_0_1_D2202

0 件の賞賛
返信
2 返答(返信)

1,891件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @SivaB,

I'm sorry for the delay.

Please find a test project attached.

I have found and reported a few issues both in RTD 1.0.1 and 2.0.0 while testing it.

 

The driver does not clear the flags correctly:

danielmartynek_0-1707399193748.png

Regardless of LVD or LVW, the driver return the same error code:

danielmartynek_1-1707399295804.png

The Power_Ip driver does not clear LVDF after POR before LVD interrupt is enabled.

 

Regards,

Daniel

 

 

0 件の賞賛
返信

1,702件の閲覧回数
HuihuiYang
Contributor I

Any sample code is available for low voltage detection interrupt for S32K144.

How to configure LVD interrupt in CT.

Used SDK version: SW32K1_S32DS_3.4.1_D2106  

タグ(1)
0 件の賞賛
返信