[s32ds]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
6,084 Views
bryan_hong
Senior Contributor I

dear nxp

I have download sdk from below.

bryan_hong_3-1732684635321.png

 

bryan_hong_0-1732683577028.png

so, I got below.

bryan_hong_1-1732683656438.png

and then, 

What can I do next? Is there any documentation for this?

I tried logging into 'example' in s32ds, can I build it ? Is there any documentation for this?

bryan_hong_4-1732684736429.png

 

2. 

What is `EB Tresos install directory` ?

bryan_hong_2-1732684617096.png

Thanks,

Bryan

0 Kudos
Reply
1 Solution
5,997 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Which example did you test?

Did you click Update Code?

Open the Peripherals perspective and click on Update Code to generate the code

Open the Peripherals perspective and click on Update Code to generate the code.jpg

View solution in original post

0 Kudos
Reply
9 Replies
5,998 Views
bryan_hong
Senior Contributor I

dear Robin

I have found  `OsIf_Cfg.h` file on `c:\NXP\S32DS.3.5\eclipse\mcu_data\components\PlatformSDK_S32K3\Base\`

but, I have meet below compilation error as below.

Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@Project_Settings/Startup_Code/exceptions.args" -MMD -MP -MF"Project_Settings/Startup_Code/system.d" -MT"Project_Settings/Startup_Code/system.o" -o "Project_Settings/Startup_Code/system.o" "../Project_Settings/Startup_Code/system.c"
../src/main.c:26:10: fatal error: CDD_Bms_SpiIf.h: No such file or directory
26 | #include "CDD_Bms_SpiIf.h"
| ^~~~~~~~~~~~~~~~~
compilation terminated.
In file included from C:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/include/Mcal.h:65,
from ../Project_Settings/Startup_Code/exceptions.c:41:
C:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory
45 | #include "OsIf_Cfg.h"
| ^~~~~~~~~~~~
compilation terminated.
make: *** [src/subdir.mk:20: src/main.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Project_Settings/Startup_Code/subdir.mk:42: Project_Settings/Startup_Code/exceptions.o] Error 1
In file included from C:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/include/Mcal.h:65,
from ../Project_Settings/Startup_Code/system.c:47:
C:/NXP/S32DS.3.5/S32DS/software/PlatformSDK_S32K3/RTD/BaseNXP_TS_T40D34M30I0R0/include/OsIf_Internal.h:45:10: fatal error: OsIf_Cfg.h: No such file or directory
45 | #include "OsIf_Cfg.h"
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Project_Settings/Startup_Code/subdir.mk:42: Project_Settings/Startup_Code/system.o] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.

13:50:58 Build Failed. 7 errors, 0 warnings. (took 360ms)

 

Thanks,

Bryan

0 Kudos
Reply
5,998 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Which example did you test?

Did you click Update Code?

Open the Peripherals perspective and click on Update Code to generate the code

Open the Peripherals perspective and click on Update Code to generate the code.jpg

0 Kudos
Reply
5,972 Views
bryan_hong
Senior Contributor I

dear Robin

thanks for your comments, I will success compile as below.

bryan_hong_0-1732853521659.png

Thanks,

Bryan

0 Kudos
Reply
6,016 Views
bryan_hong
Senior Contributor I

dear Robin

let me know how to download below.

bryan_hong_0-1732767148067.png

Thanks,

Bryan

0 Kudos
Reply
6,013 Views
bryan_hong
Senior Contributor I

dear Robin

I got `SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304.zip`

6,059 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bryan,

Please click on the upper right corner to download BMS_SWInstalationGuide_Hvbms_2024.08.pdf.
Then refer to the section ‘4 BMS Software installation procedure’.

bryan_hong_0-1732683577028.png

Why you did not download S32DS Design Studio 3.5 and S32DS Design Studio 3.5.3? Did you already install those two software?

If you want to test Bms_examples in S32DS, please click File->New->S32DS Project from Example

Create S32DS Project from Example Bms_examples.jpg

2. What is `EB Tresos install directory` ?

Please refer to How do I link EB Tresos to the S32K3 RTD Drivers

You are installing S32K3 RTD 3.0.0 used by EBTresos, so it is recommended to enter the path after installing EB_Tresos_Studio_AUTOSAR_Configuration_Tool_29_0_0. For example, C:\EB\tresos_29

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
6,043 Views
bryan_hong
Senior Contributor I

bryan_hong_0-1732754613475.png

I can't find this.

 

Why you did not download S32DS Design Studio 3.5 and S32DS Design Studio 3.5.3? Did you already install those two software?

--> yes, I have already used this 's32dk 3.5'

0 Kudos
Reply
6,036 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

HVBMS DESCRIPTION download BMS_SWInstalationGuide_Hvbms_2024.08 or 10.jpg

0 Kudos
Reply
6,021 Views
bryan_hong
Senior Contributor I

thanks quick response.

I have downloaded that!!!

0 Kudos
Reply