s32K144 FlexNVM cache is not updated.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32K144 FlexNVM cache is not updated.

2,863件の閲覧回数
wenhongkui
Contributor II
S32K144 writes to FLexNVM, and then reads it immediately, and the data will be incorrect. Read a other address and read it, will get the right result. I guess it should be that cache is not updated.
How to update the cache or temporary close of the manual FlexNVM?

2 返答(返信)

2,638件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

This happens when the DFlash prefetch buffer is not disabled in OCMDR1 register before reprogramming the data.

 

Regards,

Daniel

2,638件の閲覧回数
zky
Contributor I

Hi ,Daniel and Mr wen

I met a similar problem with you.i can access other ram but not FlexRam(0x14000000) by swd interface when i write data to these addresses,read it will be incorrect,it alway is 0x00000000,but i can write data to other ram and read from it.Would you pls do me some favor about this problem?

0 件の賞賛
返信