regarding input capture S32K144W FTM0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

regarding input capture S32K144W FTM0

1,085 Views
sandeepc
Contributor IV

Hi community i am reading the input capure from PTE8 channel (FTM0) my application is to read 20hz to 1000hz only its working fine

1) when device turned on initailly frequency measurment is possible from 20hz to 1000hz by varying with any speed

2)Let us consider iam measuring the freq of 142hz or 200hz for continiously if wire or probe cuts or function generator is turned off , i should measure the number of ticks  0 (zero) . but iam getting the number of ticks as previously measured it self instead of 0 (zero). the below function must return 0

rpm_inputcapturemeas = IC_GetMeasurement(&ic_pal_1_instanceConfig, rpm_channel);

how can i fix this issue...??

@Robin_Shen @kerryzhou @S32K_tj @S32kUser @s32k146_ige 

0 Kudos
Reply
1 Reply

1,050 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @sandeepc,

The FTM has to receive two edges before it can update the captured period / freq, until then, the function returns the old value.

But there is a callback with this event:

danielmartynek_0-1696413791023.png

The application SW can read the captured value in this callback.

Or the callback can set a SW flag every time a new value is captured, and the application SW can call IC_GetMeasurement() only when the flag is set.

 

Best regards,

Daniel

 

 

 

0 Kudos
Reply