port mcal issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

port mcal issue

2,103 次查看
yubo_guo
Contributor I

I use MCAL S32K14X_MCAL4_2_RTM_P4_1_0_1  Tresos:24.0.0 

but it shows below err

ERROR 20-08-27,17:07:57 (1803) Invalid XPath-expression for Attribute "READONLY" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/ActiveEcuC/ELEMENTS/Port/PortGeneral/PortSet2PinsDirectionApi": (35016) Cannot get a resource file for target ARM and derivate S32K14X. Maybe this is due to module restrictions. Errors "1" Warnings "21" 

pastedImage_6.png

标签 (1)
0 项奖励
回复
1 回复

2,081 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello, 

This issue is fixed in RTM 1.0.2 and above. I suggest you to use the version from 1.0.2 and above, and see whether the issue still occurs.

Best Regards,

Nam

0 项奖励
回复