openSDA USB connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

openSDA USB connection

1,474 次查看
ankan_creatara
Contributor III

Hello everyone,

I am back with some other doubts. Kindly take out some time to help me out.

I am attaching the screenshot of the opensda schematic input via USB. I have the following doubts:
1. What are these L1 and L2? I believe these are inductors. If yes, then why is its value in OHMS?
2. Why are these L1 and L2 used and connected? I understand the use of bypass capacitors along with the power source; but I couldnot figure out the use of these L1 and L2.
3. Also, kindly help me out in figuring the use of D17, D18 and D19 in the circuit.

ankan_creatara_0-1665569076916.png
Kindly help me out in understanding the schematic.

Thank you for your time.

 

0 项奖励
回复
1 回复

1,469 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) L1 and L2 are ferrite beads and 330Ohm is an impedance at 100MHz. If you want to see specific type, for instance following:
MPZ1608S331A

2) https://en.wikipedia.org/wiki/Ferrite_bead

3) It is ESD protection diode.

https://www.nexperia.com/products/esd-protection-tvs-filtering-and-signal-conditioning/esd-protectio...

0 项奖励
回复