mex config generate code different from windows and linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mex config generate code different from windows and linux

357 Views
Litten
Contributor I

The same XEM file generates different code on different systems.
Windows  file generate code normal but linux system generate abnormal
precondition:the same as RTD and SDK version install5.jpg

Tags (1)
0 Kudos
Reply
1 Reply

330 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Litten 

Currently, RTDs are supported only on the Windows platform and are not officially supported on Linux. Even if you are able to install them on Linux, you may encounter additional issues during development and integration.

One of the main reasons is that Linux is a case-sensitive operating system,  details about this situation have been discussed in the thread Problems with Lpi2c_Ip_MasterConfig and Lpi2c_Ip_SlaveState struct generation on S32DS for S32K344.

 

BR, VaneB

0 Kudos
Reply