making multiple adc hardware unit in S32DS GUI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

making multiple adc hardware unit in S32DS GUI

806 次查看
gkunalupta
Contributor III

Hi their,

I am using and in that using ADC instance 0 using NXP S32K144 Microcontroller. But of ADC instance i want to configure ADC0CH12 and ADC0CH1 with different properties in GUI.

But in GUI if i create new hardware unit but with same ADC instance number, then it shows S32Ds shows error.

 

Why is it so?? Cant i create multiple ADC hardware unit of same ADC instance but withy different features??? 

If not so is kind of limitation, but then it becomes compulsary for me to use ADC0 all channels with same configuration.

What i am having planning to have is, to have multiple hardware units of same ADC instance, so that i can configure different channels of same ADC isnatnce with differnet features. Cant i do that.

gkunalupta_0-1722202908346.png

 

标记 (3)
0 项奖励
回复
6 回复数

717 次查看
Kunal_Gettobyte
Contributor III

Any reply???

0 项奖励
回复

703 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you share your project?

0 项奖励
回复

629 次查看
gkunalupta
Contributor III

Any replies?

0 项奖励
回复

691 次查看
gkunalupta
Contributor III
 
0 项奖励
回复

776 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Which example is this related to? Also please specify used RTD/SDK. Thanks

0 项奖励
回复

753 次查看
gkunalupta
Contributor III

This is the SDK.

And no example, am creating a project from scratch.

Using ADC module Driver of Autosar RTD 1.0.0

gkunalupta_0-1722326148918.png

 

0 项奖励
回复