making multiple adc hardware unit in S32DS GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

making multiple adc hardware unit in S32DS GUI

2,306件の閲覧回数
gkunalupta
Contributor III

Hi their,

I am using and in that using ADC instance 0 using NXP S32K144 Microcontroller. But of ADC instance i want to configure ADC0CH12 and ADC0CH1 with different properties in GUI.

But in GUI if i create new hardware unit but with same ADC instance number, then it shows S32Ds shows error.

 

Why is it so?? Cant i create multiple ADC hardware unit of same ADC instance but withy different features??? 

If not so is kind of limitation, but then it becomes compulsary for me to use ADC0 all channels with same configuration.

What i am having planning to have is, to have multiple hardware units of same ADC instance, so that i can configure different channels of same ADC isnatnce with differnet features. Cant i do that.

gkunalupta_0-1722202908346.png

 

タグ(3)
0 件の賞賛
返信
6 返答(返信)

2,217件の閲覧回数
Kunal_Gettobyte
Contributor III

Any reply???

0 件の賞賛
返信

2,203件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you share your project?

0 件の賞賛
返信

2,129件の閲覧回数
gkunalupta
Contributor III

Any replies?

0 件の賞賛
返信

2,191件の閲覧回数
gkunalupta
Contributor III
 
0 件の賞賛
返信

2,276件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Which example is this related to? Also please specify used RTD/SDK. Thanks

0 件の賞賛
返信

2,253件の閲覧回数
gkunalupta
Contributor III

This is the SDK.

And no example, am creating a project from scratch.

Using ADC module Driver of Autosar RTD 1.0.0

gkunalupta_0-1722326148918.png

 

0 件の賞賛
返信