initialize the EVM board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

initialize the EVM board

2,881 Views
UnLEE
Contributor I

I successfully built S32K344_CAN_bootlloader_RTD2d0 and ran it on the EVM board. In addition, we succeeded in loading and executing S32K344_CAN_App_RTD200 through ECU-BUS.
Afterwards, if I modify the IO of S32K344_CAN_bootlloader_RTD2d0 and run it on the EVM board using the GDB Hardware Debugging tool, S32K344_CAN_App_RTD200 loaded through ECU-BUS will be executed. How do I initialize the EVM board?

0 Kudos
Reply
5 Replies

2,806 Views
UnLEE
Contributor I

As of now I have S32K344_CAN_App_RTD200 running on my EVM board. I want to run the S32K344_CAN_bootlloader_RTD2d0 program on the EVM board using the GDB Hardware Debugging tool. No matter how much I build and run it, the S32K344_CAN_App_RTD200 program continues to run. So, I want to factory reset the EVM board.

The EVM board I use is [NXP] S32K3X4EVBQ257ND.

Thank you.

0 Kudos
Reply

2,786 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @UnLEE,

What debugger do you use to erase an reload the MCU with the S32K344_CAN_bootlloader_RTD200 program?

 

BR, Daniel

0 Kudos
Reply

2,750 Views
UnLEE
Contributor I
I'm usign PEMicro Interface Debugging tool.
Thank you.
0 Kudos
Reply

2,650 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @UnLEE,

Can you share the debugging configuration?

Have you tried loading another RTD example?

What probe do you use?

 

BR, Daniel

0 Kudos
Reply

2,832 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @UnLEE,

What do you mean by the initialization?

And what EVM board do you have?

 

Thanks,

BR, Daniel

0 Kudos
Reply