i.MX8M Mini driver USB HUB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini driver USB HUB

1,860 Views
george_li
Contributor I

i.MX8M Mini can not drive USB HUB AX88772/AX88179 after i.MX8M Mini reset without USB HUB, any update driver is OK now?

Tags (1)
0 Kudos
Reply
1 Reply

1,760 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you use the i.M8MM EVK board or the board you designed yourself?

If you are using the i.M8MM EVK board reference board, the default usb is type-c port, if you want to use the usb hub you need to use the special line.

If you want to design board yourself, you need to configure the usb to host mode and then connect the hub chip.

It depend on your hardware, the i.MX8MM support usb2.0, so drive needed.

0 Kudos
Reply