flash tool for S32K142EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash tool for S32K142EVB

Jump to solution
2,297 Views
MaxSKDRN
Contributor II

Hello

Is there a tool to flash the compiled elf file on the development kit platform S32K142EVB ?

I would like to avoid to send the code to the testers, and ask them to compile and flash with S32DS IDE.

Thanks

Max

0 Kudos
Reply
1 Solution
2,291 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi MaxSKDRN,

Please refer: How to download separate .elf file to microcontroller using S32 Design Studio 

If you don't want to use S32 Design Studio, then standalone flash programmer may needed, for example:  Cyclone Programmers

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,292 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi MaxSKDRN,

Please refer: How to download separate .elf file to microcontroller using S32 Design Studio 

If you don't want to use S32 Design Studio, then standalone flash programmer may needed, for example:  Cyclone Programmers

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply