error in installing extension

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error in installing extension

Jump to solution
8,580 Views
rereli
Contributor II

version:S32DS for S32 Platform 3.4

When I install the extension"S32SDK S32K1XX RTM4.0.3"online,it says"Operation detailsSoftware being installed: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 Missing requirement: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.s32k1.s32k142w.dev.feature.feature.group [1.0.0.202106101446,1.0.0.202106101446]' but it could not be found".The screenshot is below.

So I tried to install it offline, but I searched this extension in nxp.com,there is only"S32SDK S32K1XX RTM4.0.2".

The extension"S32K1XX development package"is the same case.

how can i solve this problem?

 

1 Solution
8,304 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi @michaelcr97 and @rereli ,

Sorry for the inconvenience we bring you!

it is recommended to change Available S32DS Software Sites to https. This has been discussed in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3.

S32DS Extensions and Updates https.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

9 Replies
8,409 Views
michaelcr97
Contributor II

Hello, I get the same error when I try to install a different development package than yours, but from the same tab.

0 Kudos
Reply
8,378 Views
rereli
Contributor II
Yes,actually,i can't install every extension online in this tab.
0 Kudos
Reply
8,375 Views
michaelcr97
Contributor II

I`m trying to install those extensions offline, I will come up with updates here if I will succeed.

0 Kudos
Reply
8,371 Views
michaelcr97
Contributor II

unfortunately it didn`t worked to install it offline too

0 Kudos
Reply
8,365 Views
rereli
Contributor II
I will send an email to nxp.If i get reply, i will update here.
0 Kudos
Reply
8,305 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi @michaelcr97 and @rereli ,

Sorry for the inconvenience we bring you!

it is recommended to change Available S32DS Software Sites to https. This has been discussed in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3.

S32DS Extensions and Updates https.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

8,288 Views
rereli
Contributor II
it is useful! thanks very much
0 Kudos
Reply
8,329 Views
michaelcr97
Contributor II

Actually in my case, if I go to help->installation details-> and I expand S32Design Studio I will find that eclipse requirments market with a red "x", seems those were not installed. I attached a picture:

michaelcr97_0-1732442307684.png

 

0 Kudos
Reply
8,308 Views
rereli
Contributor II

Where is the red X.Is it?But i think it is a red + hahahah~

rereli_1-1732497776374.jpeg

 

 

0 Kudos
Reply