download hex file fail by multilink based on S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

download hex file fail by multilink based on S32DS

510件の閲覧回数
liuxing_hu
Contributor III

Hello all

I have a issue when download hex file by multilink based on S32DS

Version: 2018.R1

I try to flash hex file by clicking the following button

 

liuxing_hu_1-1709813995025.png

the following error occurs:

liuxing_hu_3-1709814180038.png

I tried disconnecting and reconnecting the hardware at every point, this issues still exist.

 

 

タグ(1)
0 件の賞賛
返信
3 返答(返信)

492件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @liuxing_hu 

First, make sure you have the latest firmware on your multilink. 

Second, make sure no other software is running that may be using the P&E interface and ports. For example, any P&E software, utilities, or another instance of a debug session. The multilink can only talk to one connection at a time.

Third, verify that your computer is detecting the debugger. This can be done using Device Manager -> Ports (COM & LPT). 

By last, make sure that your hardware is correctly connected. You can consult our recommendations in the AN5426: Hardware Design Guidelines for S32K1xx.

 

B.R.

VaneB

0 件の賞賛
返信

489件の閲覧回数
liuxing_hu
Contributor III

Hello VaneB

Thanks for your response!

First, make sure you have the latest firmware on your multilink. 

- why shall latest firmware be used? what's the version of latest firmware?

Third, verify that your computer is detecting the debugger. This can be done using Device Manager -> Ports (COM & LPT). 

- you can see the computer have detected the debugger,but not Ports, it's Jungo, is it ok?

 

liuxing_hu_1-1709888600023.png

 

 

タグ(1)
0 件の賞賛
返信

449件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi  @liuxing_hu 

Why shall the latest firmware be used? what's the version of the latest firmware?

Updating firmware in the field is often a necessary part of a product life cycle.

You can see the computer has detected the debugger, but not Ports, it's Jungo, is that ok?

Sorry for the misunderstanding, I confuse the detection of the S32 Debug Prob with this device. Yes, it is ok as Jungo.

0 件の賞賛
返信