about s32 design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about s32 design studio

943 Views
deepa5
Contributor I

hello team,

i am already using s32ds v3.4,but i want v3.5,how to upgrade version of ide if possible,shall i use two different version of ide.

0 Kudos
Reply
1 Reply

918 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please download S32 Design Studio 3.5 – Windows/Linux from S32 Design Studio for S32 Platform.  

If you can't see the email with the activation code, you can still look for it under your NXP account through the NXP Semiconductors page.
Go into "My NXP Account > Apps and Services > Activate my Software > View accounts > Select S32 Design Studio for S32 Platform v3.5". Once there, select "License Keys" and the activation code for your machine should be present.

You can install S32DS v3.4 and v3.4 at the same time. You can also install multiple S32K3 RTD versions of S32DS v3.5 at the same time(for example S32DS.3.5_RTD300 \ S32DS.3.5_RTD400).


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply