Why PIT is needed in S32K?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why PIT is needed in S32K?

1,151 次查看
deepika_16
Contributor I

Why PIT is needed for partition of clock gating even though we are having STM timers based on core clock frequency we are supplying the clock to STM?

0 项奖励
回复
1 回复

1,134 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @deepika_16,

PIT decrements from set value to zero and STM increments from zero to set value.

Also, all the PIT instances are capable of generating periodic triggers. PIT triggers are routed to motor control IPs such as eMIOS, LCU, BCTU, ADC etc. via TRGMUX. It also contains RTI which can be used for waking up from STOP mode and PIT can be used to trigger DMA.

Best regards,
Julián

0 项奖励
回复