What's the difference between these libraries?NewLib, NewLib Nano, EWL, and EWL Nano

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What's the difference between these libraries?NewLib, NewLib Nano, EWL, and EWL Nano

ソリューションへジャンプ
4,757件の閲覧回数
weekbbg
Contributor I

When I set up the project with S32DS, I found four libraries: NewLib, NewLib Nano, EWL and EWL Nano. Is there any difference between these libraries?

0 件の賞賛
返信
1 解決策
4,750件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi weekbbg,

You can refer the answer in: library selection when creating S32R274 project

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,751件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi weekbbg,

You can refer the answer in: library selection when creating S32R274 project

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信