Hi,
I'm trying to get S32K waked-up from VLPS using CMP in round robin mode. Here are the steps that I did:
- Configure SIRC divider to 2 and enable it, so I have 4 Mhz as SIRCDIV2 CLK.
- Enable clock gated LPTMR0.
- LPTMR0 is configured tu use SIRCDIV2 clk in free runing counter with CMR=0
- Configure CMP0 in round robin mode with:
/* IN0, from the 8-bit DAC output
* IN1, from the analog 8-1 mux
* Enable Channel 0, 1 and 5 for round robin
* Enable DAC
* Supply voltage reference is Vin1
* 1 round-robin clock cycle later, the result is sampled
* Compare result is 0 initial values for all channels
* From datasheet: Initialization delay for CMP in Low-speed mode is 30us max
* round robin clock is 2 MHz --> INITMOD = 30000/500 = 60
* Low Speed (LS) comparison mode is selected.
* Analog Comparator is enabled
* Clear CMP inputs changed flags
/*
* Enable Round robin
* Enable round robin interrupt
*/
CMP0->C2 |= CMP_C2_RRE(1) | CMP_C2_RRIE(1);
/* Clear TCF */
LPTMR0->CSR |= LPTMR_CSR_TCF(1u);
/* Enable LPTMR0 */
LPTMR0->CSR |= LPTMR_CSR_TEN(1u);
Am I missing something?
Is there any example how to configure LPTMR0 to trigger CMP in round robin?
Thanks
Youssef
已解决! 转到解答。
Hi Daniel,
Yes I found out that this was a mistake. I fixed the issue by Setting CMR to a value to define the trigger period. The CMP now works correctly in round robin mode. I can wake up the MCU from VLPS when cmp inputs change..
Regards,
Youssef